- System consistently delivers high-quality performance with optimized accessibility, expanded applications, and enhanced ease of use
- Small footprint enables easy transfer and use across all clinical departments1
Siemens Healthineers has launched the ACUSON Juniper, a new ultrasound system with advanced applications and imaging performance while featuring a lightweight, ergonomic design and complete maneuverability for use across a wide variety of clinical segments. Though small in size, the ACUSON Juniper does not compromise in performance, offering providers a system that is not only powerful, but nimble in design.
Siemens Healthineers incorporated feedback from the 365 participants in its largest-ever ultrasound co-creation project to ensure that the ACUSON Juniper meets the needs of today’s changing healthcare landscape. The system’s versatility and adaptability makes it ideal for diverse patient anatomies and physiologies. Users can customize the ACUSON Juniper based on patient interactions for improved clinical workflow.
“We’ve created a system that enables customers to transform care delivery and improve the patient experience by adapting to the needs of the ultrasound user,” says Peter Pellerito, Head of Siemens Healthineers Ultrasound North America. “The ACUSON Juniper’s nimble, versatile design affords healthcare providers the flexibility to utilize the system throughout all clinical departments while maintaining high-quality imaging capabilities.”
Where Form Meets Function
The ACUSON Juniper’s LED monitor and touch panel are the largest in its segment.1 The system’s two standard USB ports enable quick transfer of images to patients, eliminating the need for print-out documentation. Further improving the patient experience, the ACUSON Juniper is 40 percent quieter than other ultrasound systems in its class. Additionally, a protective sheet is available for the system’s key pad, to facilitate the reading and use of the controls while in a sterile environment such as the operating room. This protective skin can be disinfected for reuse.
Small on the Outside, Big on the Inside
1 Data on file
Contact for journalists
Theresa Gombar, Siemens Healthineers
Phone: +1 610-448-6370; Email: Theresa.Gombar@siemens-healthineers.com
Siemens Healthineers is the separately managed healthcare business of Siemens AG enabling healthcare providers worldwide to achieve better outcomes at lower costs by empowering them on their journey towards expanding precision medicine, transforming care delivery, improving patient experience and digitalizing healthcare. A leader in medical technology, Siemens Healthineers is constantly innovating its portfolio of products and services in its core areas of diagnostic and therapeutic imaging and in laboratory diagnostics and molecular medicine. Siemens Healthineers is also actively developing its digital health services and enterprise services.
In fiscal 2017, which ended on September 30, 2017, Siemens Healthineers generated revenue of €13.8 billion and profit of €2.5 billion and has about 48,000 employees worldwide. Further information is available at www.siemens.com/healthineers