Siemens Healthineers Announces First U.S. Install of SOMATOM go.Top CT Scanner

Malvern, PA|09/18/2018

• Ohio State University Wexner Medical Center acquires latest addition to SOMATOM go. CT platform, which addresses advanced clinical fields and applications

The Ohio State University Wexner Medical Center in Columbus recently became the first health care facility in the United States to install the new SOMATOM go.Top computed tomography (CT) system from Siemens Healthineers. The 128-slice scanner expands the SOMATOM go. CT platform’s concept of patient-centric mobile workflow – which is controlled via tablet and remote – into advanced clinical fields and applications, including cardiology, CT-guided intervention, and Dual Energy spectral imaging.

In addition to a 0.33-second rotation time, Stellar detector technology, and a robust 75 kW generator, the SOMATOM go.Top has a large detector with an acquisition speed of up to 175 mm in one second and an automated workflow. The system can deliver new levels of radiation dose personalization due to its high power and low kV scanning mode, along with automated tools that take the guesswork out of low-dose CT imaging. And with the system’s mobile, tablet-based workflow and the capability to off-load manual reconstruction tasks, technologists can spend more time focused on the patient.

Explaining his facility’s decision to select the SOMATOM go.Top, Richard D. White, MD, Chairman of the Department of Radiology at The Ohio State University Wexner Medical Center, said, “We were looking for an application of robust, tablet-based capabilities facilitating direct patient engagement and partnership while leveraging automated workflows to significantly reduce exam variability and error risk, as well as increase patient-specific image quality.” ¹

The Ohio State Wexner Medical Center is also using the system’s Twin Beam Dual Energy capabilities to perform dose-neutral dual energy scans that support oncological workups for patients receiving cancer care. Finally, the Ohio State team is using a new feature of SOMATOM go. scanners – Guide&GO, the first tablet-based solution for CT-guided interventional work – to enable touch screen control in the intervention suite.¹

“Siemens Healthineers is proud to provide The Ohio State University Wexner Medical Center with the nation’s first SOMATOM go.Top,” said Douglas Ryan, Vice President of Computed Tomography at Siemens Healthineers North America. “Not only can the system help transform the delivery of patient care with its dramatic changes to workflow and reliability, but it also can help achieve a new level of precision medicine.”

¹ The statements by Siemens Healthineers customers described herein are based on results that were achieved in the customer's unique setting. Because there is no "typical" hospital or laboratory and many variables exist (e.g., hospital size, samples mix, case mix, level of IT and/or automation adoption) there can be no guarantee that other customers will achieve the same results.

For further information on the SOMATOM go.Top, please see
www.usa.siemens.com/somatom-go-top

Contact for journalists
Jeff Bell
Phone: (484) 868-8346; Email: jeffrey.t.bell@siemens-healthineers.com

Siemens Healthineers enables healthcare providers worldwide to increase value by empowering them on their journey towards expanding precision medicine, transforming care delivery, improving patient experience and digitalizing healthcare. A leader in medical technology, Siemens Healthineers is constantly innovating its portfolio of products and services in its core areas of diagnostic and therapeutic imaging and in laboratory diagnostics and molecular medicine. Siemens Healthineers is also actively developing its digital health services and enterprise services.
In fiscal 2017, which ended on September 30, 2017, Siemens Healthineers generated revenue of €13.8 billion and profit of €2.5 billion and has about 48,000 employees worldwide. Further information is available at www.siemens-healthineers.com

Subscription Button Icon
Be the first to know about our events, training, and news