FDA Clears SOMATOM Edge Plus CT System from Siemens Healthineers

Malvern, PA |  Wed Apr 04 00:00:00 CEST 2018

• Premium CT system leverages artificial intelligence to automatically safeguard precise, consistent patient positioning

 

The U.S. Food and Drug Administration (FDA) has cleared the SOMATOM Edge Plus computed tomography (CT) system from Siemens Healthineers, which features the FAST (Fully Assisting Scanner Technologies) Integrated Workflow with the FAST 3D Camera – the first patient positioning system powered by artificial intelligence. Additionally, the new scanner allows for automated scan preparation, improved diagnostic confidence, and customized patient dose, making it ideal for high-volume practices and emergency imaging environments.

 

Optimizing clinical pathways
Incorrect patient positioning in CT may lead to additional image noise or increased levels of patient radiation dose. The FAST Integrated Workflow and FAST 3D Camera of the SOMATOM Edge Plus enables accurate, reproducible patient positioning. Fixed above the patient table, the FAST 3D Camera uses infrared technology and artificial intelligence to recognize anatomical landmarks. The table then aligns to the correct position to scan the body region at isocenter based on the selected protocol. This means institutions can streamline image quality, reduce dose, and potentially reduce repeat scans.

 

Improving diagnostic accuracy
Equipped with TwinBeam Dual Energy, the 128-slice SOMATOM Edge Plus enables quantitative imaging and improved tissue characterization for diagnostic confidence. This additional information allows for precise visualization of iodine uptake in a tumor. The system’s split filter technology permits acquisition of two spectral energies for dose-neutral Dual Energy scans in clinical routine. Using this technology, providers may be able to reduce additional noncontrast scans by producing virtual noncontrast images based on the Dual Energy data.

 

Personalized imaging
The SOMATOM Edge Plus enables scanning of obese patients with strong diagnostic confidence due to its Straton MX Sigma X-ray tube, high power reserves at every kV value in 10-kV increments, and the Stellar Infinity detector – resulting in sharp, high-contrast images at high speed and low dose. Tin Filter technology, which can be used in all routine examinations, enables CT scans at very low doses by shielding patients from clinically irrelevant radiation. In the case of CT lung scanning, for example, this technology enables scanning at levels associated with a standard X-ray examination.

 

“Siemens Healthineers is excited about the potential of the SOMATOM Edge Plus with FAST Integrated Workflow to help healthcare providers improve workflow and patient management,” said Douglas Ryan, Vice President of Computed Tomography at Siemens Healthineers North America. “The integration of artificial intelligence into patient positioning not only improves image quality but also expands precision medicine by reducing unnecessary variability for healthcare providers.”

 


For further information on the SOMATOM Edge Plus, please see www.usa.siemens.com/somatom-edge-plus

 

Contact for journalists
Jeff Bell
Phone: (484) 868-8346; Email: jeffrey.t.bell@siemens-healthineers.com

 

Siemens Healthineers enables healthcare providers worldwide to increase value by empowering them on their journey towards expanding precision medicine, transforming care delivery, improving patient experience and digitalizing healthcare. A leader in medical technology, Siemens Healthineers is constantly innovating its portfolio of products and services in its core areas of diagnostic and therapeutic imaging and in laboratory diagnostics and molecular medicine. Siemens Healthineers is also actively developing its digital health services and enterprise services.
In fiscal 2017, which ended on September 30, 2017, Siemens Healthineers generated revenue of €13.8 billion and profit of €2.5 billion and has about 48,000 employees worldwide. Further information is available at www.siemens-healthineers.com.

 


 


Share this page: