FDA Clears New Version of SOMATOM Force CT System from Siemens Healthineers

Malvern, PA|04/14/2018

• Premium dual source scanner includes FAST 3D Camera to automatically safeguard precise, consistent patient positioning


The U.S. Food and Drug Administration (FDA) has cleared the latest version of the SOMATOM Force, the flagship dual source computed tomography (CT) system from Siemens Healthineers. The system now features the new FAST (Fully Assisting Scanner Technologies) Integrated Workflow, which helps ensure precise patient positioning. A key component of the FAST Integrated Workflow is the all-new FAST 3D Camera, which fits above the patient table and uses artificial intelligence and deep learning to enable automatic, precise, and consistent isocentric positioning of patients. Touch Panels fitted on the gantry allow staff to leverage this automation at the push of a button while remaining close to the patient during scan preparation.


The new SOMATOM Force also offers iterative metal artifact reduction (iMAR), enabling users to significantly reduce artifacts caused by metal implants, artificial joints, or pacemakers. Additionally, the improved Image Reconstruction System (IRS) of the SOMATOM Force reconstructs up to 70 images per second with iterative reconstruction. The new FAST Integrated Workflow with the FAST 3D Camera also will be available with the SOMATOM Drive dual source CT system.


For further information on the SOMATOM Force, please see http://usa.siemens.com/somatom-force


Contact for journalists
Jeff Bell
Phone: (484) 868-8346; Email: jeffrey.t.bell@siemens-healthineers.com


Siemens Healthineers enables healthcare providers worldwide to increase value by empowering them on their journey towards expanding precision medicine, transforming care delivery, improving patient experience and digitalizing healthcare. A leader in medical technology, Siemens Healthineers is constantly innovating its portfolio of products and services in its core areas of diagnostic and therapeutic imaging and in laboratory diagnostics and molecular medicine. Siemens Healthineers is also actively developing its digital health services and enterprise services.
In fiscal 2017, which ended on September 30, 2017, Siemens Healthineers generated revenue of €13.8 billion and profit of €2.5 billion and has about 48,000 employees worldwide. Further information is available at www.siemens-healthineers.com.

Subscription Button Icon
Be the first to know about our events, training, and news