Today, Siemens Healthcare announced an agreement to enhance the syngo® Workflow radiology information system (RIS) by incorporating eXposure, which is a comprehensive radiation dose management and reporting solution from Radimetrics, Toronto. When combined with syngo Workflow RIS, the solution automatically captures the radiation dose information in a diagnostic report without any additional clicks or dictation, saving time for the radiologist. This solution is only available in the United States.
There is an increased emphasis on radiation safety, especially in the United States, that has created the need for better dose tracking and monitoring tools. Through this integration, Siemens and Radimetrics will allow hospitals and imaging centers to more easily comply with these types of dose monitoring requirements, and automatically capture radiation dose information without adding extra workflow steps. The integrated solution provides an extensive set of features such as a Cumulative Dose Tracking Scorecard, a Dosimetry Worksheet that incorporates an advanced simulation engine, Protocol Management Tools with support for multiple scanners, and Dose Reporting Dashboards with customized data views.
For more information about syngo Workflow, please visit: www.usa.siemens.com/syngoworkflow.
Launched recently, Siemens Agenda 2013 program is a two-year global initiative to further strengthen the Healthcare Sector's innovative power and competitiveness. Specific measures will be implemented in four fields of action: Innovation, Competitiveness, Regional Footprint, and People Development.
The Siemens Healthcare Sector is one of the world's largest suppliers to the healthcare industry and a trendsetter in medical imaging, laboratory diagnostics, medical information technology and hearing aids. Siemens offers its customers products and solutions for the entire range of patient care from a single source – from prevention and early detection to diagnosis, and on to treatment and aftercare. By optimizing clinical workflows for the most common diseases, Siemens also makes healthcare faster, better and more cost-effective. Siemens Healthcare employs some 51,000 employees worldwide and operates around the world. In fiscal year 2011 (to September 30), the Sector posted revenue of 12.5 billion euros and profit of around 1.3 billion euros. For further information please visit: www.siemens.com/healthcare.