The Diagnostics Division of Siemens Healthcare announces today the availability of two new advanced urine testing solutions for U.S. central laboratories—the CLINITEK Novus Automated Urine Chemistry Analyzer and the CLINITEK AUWi PRO Automated Urine Workstation.
Recently FDA-cleared and available globally, the CLINITEK Novus Analyzer delivers improved performance using proven dry-pad urine chemistry technology along with an easy-to-use urinalysis strip cassette test format to help laboratories produce reliable, trusted test results while maximizing productivity. The CLINITEK AUWi PRO System, also available in Puerto Rico and Canada, combines the CLINITEK Novus Analyzer with the Sysmex UF-1000i Urine Cell Analyzer, enabling reliable, integrated urine chemistry and sediment testing on a single platform for true walkaway capability.
Urinalysis plays a key role in the central lab setting as a non-invasive, cost effective method for detecting such conditions as early kidney disease, urinary tract infections, and liver dysfunction. Due to increasing urinalysis testing volumes, central and reference laboratories are looking to automate and maximize productivity of their urine testing processes, including options to integrate urine chemistry and sediment testing for even greater workflow efficiency.
“With the growing demands in urine testing, customers need easy-to-operate instruments that can manage a broad spectrum of tests and produce reliable results, while handling peak times effortlessly,” said David Stein, PhD, CEO, Point of Care Business Unit, Siemens Healthcare Diagnostics. “Our latest solutions build upon Siemens’ proven track record in urinalysis testing to meet these strict benchmarks. We are able to provide our customers with broad clinical insight into their patients’ health while enhancing their productivity and streamlining workflow.”
Since urinalysis samples come from a variety of collection sites (nursing homes, outpatient clinics, emergency departments) at all times of the day and night, laboratories need a simple solution, like the CLINITEK Novus Analyzer, to manage high volumes while delivering consistent, reliable results. As a standalone system with a full range of tests, the CLINITEK Novus Analyzer builds on the foundation created by the CLINITEK Atlas analyzer. The CLINITEK Novus Analyzer simplifies routine analysis and features a new digital imaging measurement system to improve results accuracy. Also, automatic entry of cassette lot numbers and expiration dates, as well as new design elements, such as a tiltable color-touch screen, intuitive user interface, and customizable menu options, enhance ease of use.
For labs seeking to further automate their urine testing workflow, there’s the CLINITEK AUWi PRO System, facilitating automatic sample transport between the CLINITEK Novus workstation and Sysmex UF-1000i – a urine sediment analyzer featuring two reaction chambers for improved sensitivity to bacteria and more accurate sediment classification. By enabling one-touch urinalysis testing and minimizing manual processes, the CLINITEK AUWi PRO System allows labs to work more efficiently. Plus, with automatic verified results reported directly to the laboratory information system (LIS), the need for technician follow-up is minimized.
For further information about the CLINITEK Novus System and CLINITEK AUWi PRO System, please visit http://usa.healthcare.siemens.com/urinalysis.
Contact for journalists
Susan Drew
Siemens AG Healthcare
Phone: +1 914-524-2844; E-mail: susan.drew@siemens.com
Follow us on Twitter at: www.twitter.com/siemenshealth
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is No. 1 in offshore wind turbine construction, a leading supplier of combined cycle turbines for power generation, a major provider of power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2014, which ended on September 30, 2014, Siemens generated revenue from continuing operations of €71.9 billion and net income of €5.5 billion. At the end of September 2014, the company had around 357,000 employees worldwide. Further information is available on the Internet at http://www.siemens.com.