· New, easy-to-use, hand carried, ultrasound system suitable for an emergency department that handles a large volume of complex cases
At this year’s American College of Emergency Physicians (ACEP), October 26-29 in Boston, Siemens Healthcare introduces its new hand-carried ACUSON P500™ ultrasound system, FROSK edition. Its reliable and fast imaging through new and time-tested high-end imaging technology in a compact and easy-to-use device, makes it particularly suitable for use in the emergency department.
All this comes in a compact notebook format of 15-inches (38 cm). Equipped with a battery that offers up to 60 minutes of scanning time, the new platform can be easily carried and positioned in any clinical environment, helping clinicians make quick decisions even in difficult scanning conditions. With a standard rapid boot-up feature, the system is ready for scanning in less than 30 seconds.
Ideal for those seeking simplicity
The ACUSON P500™ system’s clear user interface is easy to learn and operate for users of all experience levels. It features a highly sensitive touch screen display with advanced infrared (IR) technology for accurate gesturing. A dual interface control panel offers flexible use of the touch screen or a traditional control panel based on each user’s own scanning preferences, allowing them to spend less time on the system and more time on the patient.
“The P500 is simple but not simplistic. Novice sonographers will appreciate its intuitive, easy-to-use interface, whereas more sophisticated users will enjoy the state-of-the-art features available”, says Adam J. Ash, DO, RDMS Associate Director, Department of Emergency Medicine, St. Joseph Hospital, Beth Page, NY. “The dynamic persistence and color artifact suppression technologies make doppler imaging much more accessible, and the inclusion of continuous wave doppler allows those interested to perform truly advanced cardiac studies.”
For rapid, reliable visualization, the ACUSON P500™ ultrasound system, FROSK edition is highly portable. A small footprint enables easy navigation through cramped ED spaces while superior engineering provides high-quality imaging when and where it’s needed, for greater clinical confidence and speed to treatment.
Contact for journalists:
Carly Heimer
Siemens Healthcare
Phone: 610-448-6347; E-mail: carly.heimer@siemens.com
Follow us on Twitter at: www.twitter.com/siemenshealth
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is No. 1 in offshore wind turbine construction, a leading supplier of combined cycle turbines for power generation, a major provider of power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2014, which ended on September 30, 2014, Siemens generated revenue from continuing operations of €71.9 billion and net income of €5.5 billion. At the end of September 2014, the company had around 357,000 employees worldwide. Further information is available on the Internet at http://www.siemens.com.