· Highly flexible system optimized for broad clinical utilization installed at Detroit’s St. John Hospital and Medical Center
St. Johns Hospital and Medical Center in Detroit recently became the first U.S. health care facility to install the Artis one angiography system from Siemens Healthcare. The Artis one is designed to address a broad range of angiographic procedures, from diagnosing and treating coronary artery disease and peripheral vessel occlusions to performing electrophysiology procedures. St. Johns is using the Artis one primarily for interventional cardiology and electrophysiology.
“The compact nature of the Artis one angiography system makes it easy to work with,” says Lingareddy Devireddy, MD, FACC, CCDS, medical director of cardiology services and chief of cardiology at St. Johns Providence Health System, Warren, Mich. “The footprint of the base and its movement make it easy for left-sided implants, and the system’s peristepping function is convenient for peripheral work.”
Enjoying a positioning flexibility similar to ceiling-mounted systems, the Artis one occupies just 269 square feet, compared to the standard 484 square feet required by ceiling-mounted systems. The Artis one has multiple axes capable of moving independently of one another, enabling easy positioning of the system where needed – regardless of where the user is standing. The system accommodates head-to-toe coverage of patients up to 6 feet, 10 inches without the need for patient repositioning. Artis one’s Clearstent Live application for interventional cardiology procedures – previously available only with Siemens’ premium family Artis Q and Artis Q.zen – freezes motion in the stent region, allowing the physician to mask out movement of the beating heart and place the stent in precisely the correct position. Cardiac imaging tools of the Artis one include HeartSweep, which uses dual-axis rotational angiography to image the entire heart in one smooth C-arm movement to potentially speed up procedures and save contrast agents.1 By utilizing 20 percent less energy than Siemens’ Artis zee floor system, the Artis one also helps reduce operational costs.
The statements by Siemens customers described herein are based on results that were achieved in the customer’s unique setting. Since there is no “typical” hospital and many variables exist (e.g., hospital size, case mix, level of IT adoption), there can be no guarantee that other customers will achieve the same results.
Contact for journalists:
Jeffrey Bell
Siemens AG Healthcare
Phone: +1 610-448-1477; E-mail: jeffrey.t.bell@siemens.com
For further information on the Artis one, please see www.usa.siemens.com/artis-one
Follow us on Twitter at: www.twitter.com/siemenshealth
The Siemens Healthcare Sector is one of the world's largest suppliers to the healthcare industry and a trendsetter in medical imaging, laboratory diagnostics, medical information technology and hearing aids. Siemens offers its customers products and solutions for the entire range of patient care from a single source – from prevention and early detection to diagnosis, and on to treatment and aftercare. By optimizing clinical workflows for the most common diseases, Siemens also makes healthcare faster, better and more cost-effective. Siemens Healthcare employs some 52,000 employees worldwide and operates around the world. In fiscal year 2013 (to September 30), the Sector posted revenue of 13.6 billion euros and profit of 2.0 billion euros. For further information, please visit: www.siemens.com/healthcare