Siemens Announces First U.S. Installation of MAGNETOM Prisma 3T MRI System

05/02/2014

· New 3T MRI scanner capable of ultra-high spatial and temporal resolution installed at University of Minnesota’s Center for Magnetic Resonance Research

The Center for Magnetic Resonance Research (CMRR) at the University of Minnesota, Minneapolis, is the first U.S. facility to install the MAGNETOM Prisma, a 3 Tesla (3T) magnetic resonance imaging (MRI) scanner from Siemens Healthcare capable of exceptionally high spatial and temporal resolution to achieve outstanding image quality, particularly in highly demanding situations.

“The Center for Magnetic Resonance Research is excited to add the MAGNETOM Prisma 3T scanner to support our research efforts to obtain better information about anatomical connections within the brain.” said Kamil Ugurbil, PhD, director of CMMR and a professor in the departments of Radiology, the Neurosciences, and Medicine at the University of Minnesota. “The large gradient strength in the Prisma provides the potential for us to encode the diffusion of water in the brain much more quickly than conventional MRI scanners, yielding signal-to-noise gains that increase image resolution and enhance our ability to detect smaller effects in the brain.”

The MAGNETOM Prisma possesses XR Gradients, which combine 80 milliTesla per meter (m/T/m) with a 200T-per-meter-per-second (T/m/s) slew rate within one sequence for a configuration not found on any other commercial whole-body MR system. Complementing the extraordinary power of the MAGNETOM Prisma’s XR Gradients is the system’s highly robust design, which enables precision to be maintained through long, demanding applications such as functional MRI (fMRI). The power and endurance of the MAGNETOM Prisma’s XR Gradients fuel the system’s first-to-market Diffusion Spectrum Imaging (DSI) acquisition, which enables the user to potentially resolve fine anatomical details of the brain such as crossing white-matter fibers.

Further enhancing the MAGNETOM Prisma’s image quality is the scanner’s benchmark homogeneity and advanced shimming solutions that allow for finer, more effective compensation of patient-induced field disturbances. Combined, these features offer the user an outstanding basis for cardiac and body imaging, as well as applications such as spectroscopy.

The MAGNETOM Prisma possesses Siemens’ Dot (Day optimizing throughput) engines, which enable the high level of consistency that is crucial for both research applications and demanding clinical work. The Dot engine brings automation and reproducibility to investigations across subjects, time points, and institutions to raise the integrity of longitudinal studies and multi-site research projects.


Contact for journalists:

Jeff Bell
Siemens Healthcare
Phone: +1 610-448-1477; E-mail: jeffrey.t.bell@siemens.com

For further information on the MAGNETOM Prisma, please see http://usa.healthcare.siemens.com/medical-imaging/magnetic-resonance-imaging/3t-mri-scanner/magnetom-prisma

Follow us on Twitter: www.twitter.com/siemenshealth

The Siemens Healthcare Sector is one of the world's largest suppliers to the healthcare industry and a trendsetter in medical imaging, laboratory diagnostics, medical information technology and hearing aids. Siemens offers its customers products and solutions for the entire range of patient care from a single source – from prevention and early detection to diagnosis, and on to treatment and aftercare. By optimizing clinical workflows for the most common diseases, Siemens also makes healthcare faster, better and more cost-effective. Siemens Healthcare employs some 52,000 employees worldwide and operates around the world. In fiscal year 2013 (to September 30), the Sector posted revenue of 13.6 billion euros and profit of 2.0 billion euros. For further information please visit: www.siemens.com/healthcare

Subscription Button Icon
Be the first to know about our events, training, and news