· New 16-slice system designed for clinical routine
· Available in two power configurations to better meet clinical, workflow requirements
Siemens Healthcare has announced that the Food and Drug Administration (FDA) has cleared the SOMATOM Scope, a new 16-slice computed tomography (CT) scanner. The SOMATOM Scope delivers the image quality, dose reduction and workflow-enhancing benefits long associated with the SOMATOM family of CT scanners at a price point that enables facilities to extend routine diagnostic imaging services to more patients and in more specialty settings. The SOMATOM Scope also includes eCockpit technology that extends the scanner’s operational lifetime by minimizing wear and tear on its most vital components. Designed for private radiology practices, community hospitals, critical access hospitals, specialty practices such as orthopedics and urology, and veterinary medicine, the SOMATOM Scope is available in two configurations – Scope and Scope Power – and enables healthcare providers to comply with the NEMA XR-29 Smart Dose Standard, ensuring a safer imaging experience for patients.
“By adding the Scope to our portfolio of SOMATOM CT scanners, we help bring CT imaging closer to the point of care, enabling our customers to focus on what matters the most: improving care through more informed, timely clinical decision-making,” said Murat Gungor, vice president, computed tomography and radiation oncology business management at Siemens Healthcare. “The SOMATOM Scope helps to ensure that a greater segment of the patient population has access to innovative technologies while enabling facilities to help control costs as well as save time and effort throughout their daily routine.”
While the SOMATOM Scope is designed for use in routine diagnostic imaging as well as oncological examinations, interventional radiology, and vascular imaging, the more robust SOMATOM Scope Power – with its stronger X-ray tube, higher performance generator, and faster rotation speed – is ideal for higher volume clinical settings. The SOMATOM Scope utilizes Siemens’ breakthrough IRIS (Iterative Reconstruction in Image Space) technology, which accelerates image reconstruction while reducing noise and artifacts. And the system’s Adaptive Signal Boost technology amplifies low signals when high attenuation is present. The SOMATOM Scope includes Siemens FAST (Fully Assisting Scanner Technology) and CARE (Combined Applications to Reduce Exposure) applications to help reduce radiation exposure and standardize the CT imaging process – freeing up more time for technologists to interact with patients.
The SOMATOM Scope’s lightweight nature and extremely low space requirement of 130.2 sq. ft. enable installation in nearly any room. Energy-saving functions reduce its energy consumption and enable facilities to save on air conditioning due to low heat emissions. Additionally, the system’s eCockpit technology package includes eSleep, which helps to further reduce energy costs by putting the gantry into eSleep mode during periods of extended inactivity. The eCockpit’seMode (previously available only on the SOMATOM Perspective CT system), enables the scanner to automatically select the optimum scan parameters, curbing wear and tear on the hardware. And with the eCockpit’s eStart feature, the user can extend the lifespan of the system’s X-ray tube through a gradual warm-up process following longer periods of stand-by status.
Contact for journalists:
Jeff Bell
Siemens Healthcare AG
Phone: +1 610-448-1477; E-mail: jeffrey.t.bell@siemens.com
For further information on the SOMATOM Scope, please see www.usa.siemens.com/CT
Follow us on Twitter: www.twitter.com/siemenshealth
The Siemens Healthcare Sector is one of the world's largest suppliers to the healthcare industry and a trendsetter in medical imaging, laboratory diagnostics, medical information technology and hearing aids. Siemens offers its customers products and solutions for the entire range of patient care from a single source – from prevention and early detection to diagnosis, and on to treatment and aftercare. By optimizing clinical workflows for the most common diseases, Siemens also makes healthcare faster, better and more cost-effective. Siemens Healthcare employs some 52,000 employees worldwide and operates around the world. In fiscal year 2013 (to September 30), the Sector posted revenue of 13.6 billion euros and profit of 2.0 billion euros. For further information, please visit: www.siemens.com/healthcare