· New high-performance dual source CT scanner enables precise diagnostics in pediatrics, cardiology, oncology, and emergency medicine
· System’s new tin filter and low-voltage capabilities help to reduce patient X-ray dose and required dose of contrast media
Siemens Healthineers has announced that the Food and Drug Administration (FDA) has cleared the SOMATOM Drive computed tomography (CT) system. This new dual source scanner is designed to drive precision in diagnostic imaging across a wide range of clinical disciplines – from pediatrics and emergency medicine to cardiology and oncology – as well as deliver a new level of quality in patient care, with the potential to reduce examination time, preparation, and follow-up care.
“Siemens Healthineers is proud to introduce the high-performance SOMATOM Drive dual source CT system, which provides our customers with the flexibility to deliver more precise imaging – and potentially further reduce patient dose through the utilization of multiple KV settings,” says Douglas Ryan, Vice President of Computed Tomography at Siemens Healthineers North America.
The SOMATOM Drive CT system is equipped with the new Straton MX Sigma X-ray tubes and Sigma generators, which allow for more targeted beam focusing and enable examinations using high energy levels at low voltages. These lower voltages may allow clinicians to use less contrast, which can be burdensome for patients who are seriously ill or have reduced kidney function. And because the X-ray tube voltages of the SOMATOM Drive are adjustable in 10 kV increments ranging from 70 kV to 140 kV, clinicians can tailor the voltage and, therefore, the dose to each patient. Scanning at a lower kV level reduces patient radiation exposure.
This technology helps enable CT lung scans to be performed at an extremely low dose, which could prove beneficial for lung cancer screening. With this combination of low doses and high diagnostic reliability, the SOMATOM Drive is also ideal for spinal diagnostics and orthopedic examinations. Additionally, the scanner’s Dual Energy mode can help clinicians accurately differentiate between tissue and bone.
Patient and user advantages
The speed of the SOMATOM Drive CT system supports pediatric CT examinations with no sedation And the system’s Stellar Infinity detector and integrated iterative reconstruction capabilities, coupled with the use of very low kV levels, support an environment where the lowest doses are used for pediatric patients.
Elderly patients who present to the hospital with undiagnosed chest pain and breathing difficulties are among the patient populations who can benefit from the ability to breathe freely during scanning with the SOMATOM Drive. And thanks to the system’s ultra-fast scanning speed, the patient’s heart and lung movement does not compromise diagnostic imaging quality. Further, since a cardiac scan can be performed in one heartbeat using the SOMATOM Drive, beta-blockers may no longer be required to slow the heartbeat of some patients.
These patient benefits also may lead to smoother workflows in the radiology department. If the clinical images from the first CT scan are of diagnostic quality, multiple scans are not necessary. For most patients with reduced kidney function, a lower dose of contrast media may reduce the need for related preparation and follow-up. And since the scanner supports the potential to preform CT examinations with no sedation, anesthetic support and additional intensive medical care may not be required.
Contact for journalists
Jeff Bell
Siemens Healthcare
Phone: (484) 868-8346 E-mail: jeffrey.t.bell@siemens-healthineers.com
Follow us on Twitter: www.twitter.com/SiemensHealth
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world’s largest producers of energy-efficient, resource-saving technologies, Siemens is No. 1 in offshore wind turbine construction, a leading supplier of gas and steam turbines for power generation, a major provider of power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2015, which ended on September 30, 2015, Siemens generated revenue of €75.6 billion and net income of €7.4 billion. At the end of September 2015, the company had around 348,000 employees worldwide. Further information is available on the Internet at www.siemens.com