· RT Pro edition enhances radiation oncology workflow on company’s SOMATOM Definition AS Open CT simulator
Siemens Healthcare has announced that the Food and Drug Administration (FDA) has cleared the RT Pro edition – a package of features designed to enhance radiation oncology workflow for Siemens’ SOMATOM Definition AS Open CT simulator. The RT Pro edition of the SOMATOM Definition AS Open helps deliver even higher image quality for all needs in radiation oncology – including large patients, patients with metal implants, and those who experience tumor motion.
Innovations in the RT Pro edition include MARIS (Metal Artifact Reduction in Image Space), which helps ensure accurate CT data for treatment planning by reducing image-distorting beam-hardening artifacts caused by a patient’s metal implants. Added to Siemens’ respiratory gating solution, the t-minIP and t-MIP features visualize tumor movement in one image, which is particularly useful when analyzing tumor motion and contouring. Also, Siemens’ HD FoV Pro algorithm uses intelligent contour and attenuation estimation to further improve visibility outside the scan field-of-view (sFoV) through the extended 80-cm FoV, ultimately increasing image accuracy for treatment planning. MARIS, t-minIP, t-MIP, and HD FoV Pro are all standard with the RT Pro edition. Finally, the previously available Dual Energy feature is included as an option on the RT Pro edition, helping to reduce metal artifacts and increase soft tissue contrast.
Contact for journalists:
Jeff Bell
Siemens Healthcare
Phone: +1 610-448-1477; E-mail: jeffrey.t.bell@siemens.com
Follow us on Twitter at: www.twitter.com/siemenshealth
The Siemens Healthcare Sector is one of the world's largest suppliers to the healthcare industry and a trendsetter in medical imaging, laboratory diagnostics, medical information technology and hearing aids. Siemens offers its customers products and solutions for the entire range of patient care from a sinwww.siemens.com/healthcaregle source – from prevention and early detection to diagnosis, and on to treatment and aftercare. By optimizing clinical workflows for the most common diseases, Siemens also makes healthcare faster, better and more cost-effective. Siemens Healthcare employs some 52,000 employees worldwide and operates around the world. In fiscal year 2013 (to September 30), the Sector posted revenue of 13.6 billion euros and profit of 2.0 billion euros. For further information please visit: www.siemens.com/healthcare.