· SEEit surface coil solution facilitates noninvasive, high-resolution prostate MR in 10 minutes without endorectal coil
The Food and Drug Administration (FDA) has cleared the noninvasive SEEit prostate magnetic resonance (MR) imaging solution from Siemens Healthcare. Powered by syngo MR E11 software architecture, SEEit enables users of Siemens’ high-performance MAGNETOM Aera 1.5 Tesla (1.5T) and MAGNETOM Skyra 3T MRI systems to perform a routine prostate exam in just 10 minutes without using an endorectal coil, which can cause patient discomfort. Siemens’ Direct RF and high-density coil technology Tim 4G – coupled with its unique RESOLVE diffusion technology – deliver the essential signal-to-noise ratio (SNR) and resolution that enable users to perform these examinations using only the company’s new Body 30/60 surface coil.
For more information, please visit www.usa.siemens.com/prostatemri
Contact for journalists
Jeff Bell
Siemens Healthcare
Phone: 610-448-6348; E-mail: jeffrey.t.bell@siemens.com
Follow us on Twitter: www.twitter.com/SiemensHealth
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world’s largest producers of energy-efficient, resource-saving technologies, Siemens is No. 1 in offshore wind turbine construction, a leading supplier of gas and steam turbines for power generation, a major provider of power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2015, which ended on September 30, 2015, Siemens generated revenue of €75.6 billion and net income of €7.4 billion. At the end of September 2015, the company had around 348,000 employees worldwide. Further information is available on the Internet at www.siemens.com