· Highly flexible system covers most angiographic procedures and provides improved patient access
· HeartSweep enables cardiac imaging from multiple projections in one sweep
Siemens Healthcare has announced that the U.S. Food and Drug Administration (FDA) has cleared the Artis one – an angiography system optimized for broad clinical utilization. The Artis one is designed for routine interventions, including revascularizations of peripheral vessel occlusions, functional tests of dialysis shunts in patients with kidney failure, diagnostic or minimally invasive angiographic treatment of narrowed coronary arteries, and pacemaker implantations.
Flexible with low space requirement
Despite being floor-mounted, the Artis one enjoys a positioning flexibility similar to ceiling-mounted systems and occupies just 269 square feet, compared to the standard 484 square feet required by ceiling-mounted systems. The system features several axes that can move independently of one other, enabling physicians and hospital staff to easily position the system where needed – regardless of where they stand. It accommodates full head-to-toe coverage of patients up to 6 feet, 10 inches without the need for patient repositioning. The system allows free access to the patient's head, enabling optimal care during the procedure.
Tactile buttons on the Artis one’s tableside console can be manipulated easily even under the sterile covering. The system’s on-screen, menu-guided user interface allows the physician to navigate directly using the heads-up display. All information regarding the procedure remains directly in front of the operator. The Artis one’s 30-inch display size delivers images up to 90 percent larger than conventional 19-inch monitors.
Premium cardio applications, powerful X-ray tube
Artis one’s Clearstent Live application for interventional cardiology procedures – previously available only with Siemens’ premium family Artis Q and Artis Q.zen – freezes motion in the region of the stent, allowing the physician to mask out movement of the beating heart and place the stent in precisely the correct position. The Artis one also offers new tools for cardiac imaging, including HeartSweep, which uses dual-axis rotational angiography to image the entire heart in a single, smooth C-arm movement instead of multiple acquisitions from different projections. This single-sweep movement has the potential to speed up procedures and save contrast agents.1 By utilizing 20 percent less energy than Siemens’ Artis zee floor system, the Artis one also helps reduce operational costs. This feat is achieved primarily through components manufactured by Siemens for industry automation.
The Artis one angiography system is available in multiple configurations that are tailored to fit a broad range of clinical requirements.
Contact for journalists:
Jeff Bell
Siemens Healthcare
Phone: +1 610 448-1477; E-mail: jeffrey.t.bell@siemens.com
Follow us on Twitter at: www.twitter.com/siemenshealth
The Siemens Healthcare Sector is one of the world's largest suppliers to the healthcare industry and a trendsetter in medical imaging, laboratory diagnostics, medical information technology and hearing aids. Siemens offers its customers products and solutions for the entire range of patient care from a single source – from prevention and early detection to diagnosis, and on to treatment and aftercare. By optimizing clinical workflows for the most common diseases, Siemens also makes healthcare faster, better and more cost-effective. Siemens Healthcare employs some 52,000 employees worldwide and operates around the world. In fiscal year 2013 (to September 30), the Sector posted revenue of 13.6 billion euros and profit of 2.0 billion euros. For further information, please visit: www.siemens.com/healthcare.