· New version of Siemens’ established digital imaging solution offers two-detector X-ray technology for smaller budgets
Siemens Healthcare has announced that a new, two-detector version of its established Multix Fusion digital radiography system has received 510(k) clearance from the Food and Drug Administration (FDA) and is now available in the United States. Supporting the full spectrum of routine radiography at an affordable price, the two-detector iteration of the Multix Fusion – a digital imaging system Siemens introduced in 2012 – features digital cassette-sized flat-panel detectors, a large fixed detector in the wall stand, a height-adjustable table with a 660-pound weight capacity, and a touch screen positioned at the overhead tube suspension for exam parameter changes at the patient’s side.
With a high level of reliability and attractive service contracts that help keep its operating costs comparatively low, the two-detector Multix Fusion is designed for customers with high patient throughput who are looking for excellent image quality at low dose. The system’s two detectors offer nearly unlimited positioning flexibility between the table and wall stand, covering routine to advanced applications such as ortho, long leg, and full spine studies. The system’s high level of image contrast is the result of its DiamondView Plus on-board post-processing tool, and the automated image processing parameter provides settings based on organ programs.
Contact for journalists
Jeff Bell
Siemens Healthcare
Phone: 610-448-1477; E-mail: jeffrey.t.bell@siemens.com
Follow us on Twitter at: www.twitter.com/SiemensHealth
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is No. 1 in offshore wind turbine construction, a leading supplier of combined cycle turbines for power generation, a major provider of power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2014, which ended on September 30, 2014, Siemens generated revenue from continuing operations of €71.9 billion and net income of €5.5 billion. At the end of September 2014, the company had around 357,000 employees worldwide. Further information is available on the Internet at http://www.siemens.com.