Scanner is designed for demanding clinical and research challenges
Siemens Healthcare has announced that the Food and Drug Administration (FDA) has cleared the MAGNETOM Prisma, a 3 Tesla (3T) magnetic resonance imaging (MRI) scanner capable of extraordinarily high spatial and temporal resolution to achieve outstanding image quality, particularly in highly demanding applications.
“Siemens is proud to add the MAGNETOM Prisma 3T scanner to our portfolio of world-class MRI systems,” says Gregory Sorensen, MD, CEO of Siemens Healthcare North America. “With applications that display functional information and enable the visualization of details in the smallest anatomical structures, the MAGNETOM Prisma enables researchers to explore bold new territories and address their specific research needs.”
The MAGNETOM Prisma features XR Gradients, which combine 80 milliTesla per meter (mT/m) with a 200T-per-meter-per-second (T/m/s) slew rate to offer a configuration unavailable in any other commercial whole-body system. Complementing the extraordinary power of the MAGNETOM Prisma’s XR Gradients is the system’s exceptionally robust design. Precision is maintained throughout long, demanding applications such as functional MRI (fMRI). The power and endurance of the MAGNETOM Prisma’s XR Gradients fuel the system’s first-to-market Diffusion Spectrum Imaging (DSI) acquisition that enables the user to potentially resolve fine anatomical details of the brain such as crossing white-matter fibers.
Image quality is further enhanced by the MAGNETOM Prisma’s benchmark homogeneity and advanced shimming solutions that allow for finer, more effective compensation of patient-induced field disturbances. Together, these features provide the user with an outstanding basis for cardiac and body imaging, as well as applications such as spectroscopy.
The MAGNETOM Prisma possesses Siemens’ Dot (Day optimizing throughput) engines that enable exceptional consistency, which is crucial both in research applications and clinical work. The Dot engine brings automation and reproducibility to investigations across subjects, time points, and institutions, raising the integrity of longitudinal studies and multi-site research projects.
Siemens will offer onsite upgrades to the MAGNETOM Prisma to customers who have already installed the MAGNETOM Trio, a 3T MRI system with Tim (Total imaging matrix) technology.
Contact for journalists:
Jeff Bell
Siemens Healthineers
Phone: +1 610-448-1477; E-mail: jeffrey.t.bell@siemens.com
For further information on the MAGNETOM Prisma, please see http://usa.healthcare.siemens.com/medical-imaging/magnetic-resonance-imaging/3t-mri-scanner/magnetom-prisma
Follow us on Twitter at: www.twitter.com/siemenshealth
The Siemens Healthcare Sector is one of the world's largest suppliers to the healthcare industry and a trendsetter in medical imaging, laboratory diagnostics, medical information technology and hearing aids. Siemens offers its customers products and solutions for the entire range of patient care from a single source – from prevention and early detection to diagnosis, and on to treatment and aftercare. By optimizing clinical workflows for the most common diseases, Siemens also makes healthcare faster, better and more cost-effective. Siemens Healthcare employs some 52,000 employees worldwide and operates around the world. In fiscal year 2013 (to September 30), the Sector posted revenue of 13.6 billion euros and profit of 2.0 billion euros. For further information please visit: www.siemens.com/healthcare.