Innovations for Imaging Education Symposium

The more you know, the better their care.

Innovations for Imaging Education Symposium
 
Contact Us

REGISTER NOW!


To register for the conference, an order number is required. There are two registration options: 

  1. Education Funds. If available, you may use or convert previously purchased, unused education funds toward attendance. Find out more by calling 1-888-221-8010, options 1 and 4, or sending an email to educationccainnovation.team@siemens-healthineers.com. You will need to have your functional location/site ID number(s) available when you make the call. You will then be given a unique order number and instructions on how to register for the conference.
  2. Registration Package. If you do not have educational funds, you will need to purchase a package to register for the symposium. Packages that include lodging and/or airfare are available. Please send an email to clinicaleducation.team@siemens-healthineers.com or call 1-888-221-8010, options 1 and 1. You will then be given a unique order number and instructions on how to register for the conference. This also applies to healthcare professionals who are paying for registration with a credit card.

 
In either option, you will be given an order number and instructions. You may then proceed to register for the conference. Please do not register for the conference until you receive further instructions and your order number.

Click here for registration fee information 0.2 MB

Please note the 2019 cancellation policy as outlined below. 

Got your order number?


REGISTER NOW!

For questions, please contact Lori Schreiber, Event Manager, via email at

loriann.schreiber@siemens-healthineers.com

2019 Cancellation Policy 

Prior to 5/8/2019 registrant is liable for all non-refundable incurred program expenses (such as airfare and/or hotel fees).
On or between 5/8/2019 and 5/14/2019 – registrant is liable for 50% of the program fee.
On or between 5/15/2019 and 5/17/19 – registrant is liable for 75% of the program fee.
On or after 5/18/19 – registrant is liable for 100% of the program fee.