MRI of the Shoulder: Utilizing the Glenoid Clockface Orientation

Steven D. Needell, M.D.
Boca Radiology Group, P.A., Boca Raton, USA
 |  Nov 22, 2011

Orthopedic surgeons describe the glenoid fossa as the face of a clock, with the longitudinal axis defined by the supraglenoid tubercle at the 12:00 position and the inferior margin of the glenoid at the 6:00 position. Orienting the shoulder MRI exam relative to this clockface is ideal as it results in images which consistently correspond with the arthroscopists’ perspective and optimally profiles the major anatomic structures of the glenohumeral joint.
In this article, Steven D. Needell, M.D. (Boca Radiology Group, P.A., Boca Raton, FL, USA) describes how to use the technique and shows its advantages in clinical cases.

The information presented is for illustration only and is not intended to be relied upon by the reader for instruction as to the practice of medicine. Any health care practitioner reading this information is reminded that they must use their own learning, training and expertise in dealing with their individual patients. This material does not substitute for that duty and is not intended by Siemens Healthcare to be used for any purpose in that regard.

The drugs and doses mentioned herein are consistent with the approval labelling for uses and/or indications of the drug. The treating physician bears the sole responsibility for the diagnosis and treatment of patients, including drugs and doses prescribed in connection with such use. The Operating Instructions must always be strictly followed when operating the system. The source for the technical data is the corresponding data sheets. Results may vary.