IMMULITE 2000/2000 XPi TSI Assay

IMMULITE 2000/2000 XPi TSI Assay
 
Contact Us

Graves’ disease is an autoimmune disorder that leads to overactivity of the thyroid gland – hyperthyroidism. It is caused by an abnormal immune system response that causes the thyroid gland to produce too much thyroid hormone. The thyroid gland is a butterfly-shaped organ that lies flat against the windpipe in the throat. It produces the hormones thyroxine (T4) and triiodothyronine (T3) and plays an important role in controlling the body's metabolism.1

What are the symptoms of Graves’ disease?2
People with Graves’ disease may have common symptoms of hyperthyroidism such as

  • nervousness or irritability
  • fatigue or muscle weakness
  • heat intolerance
  • trouble sleeping
  • hand tremors
  • rapid and irregular heartbeat
  • frequent bowel movements or diarrhea
  • weight loss
  • goiter, which is an enlarged thyroid that may cause the neck to look swollen and can interfere with normal breathing and swallowing


In addition, the eyes of people with Graves’ disease may appear enlarged because their eyelids are retracted—seem pulled back into the eye sockets—and their eyes bulge out from the eye sockets. This condition is called Graves’ ophthalmopathy.2

Who is likely to develop Graves’ disease?

Graves’ disease usually occurs in people younger than age 40 and is seven to eight times more common in women than men.2 Women are most often affected between ages 30 and 60.2
According to the National Women's Health Information Center, Graves’ disease affects about 2% of women at some time in their lives.
 

Factors such as age, sex, heredity, and emotional and environmental stress are likely involved in Graves’ disease. And a person’s chance of developing Graves’ disease increases if other family members have the disease. Researchers have not been able to find a specific gene that causes the disease to be passed from parent to child. While scientists know some people inherit an immune system that can make antibodies against healthy cells, predicting who will be affected is difficult. 2

Laboratory Testing
Laboratory testing is essential to verify the diagnosis, help estimate the severity of, monitoring, and assisting in planning therapy for Graves’ disease patients.
To detect thyroid dysfunction, testing may begin with:

  • TSH — typically low in Graves’ disease
  • Total or free T4 — usually elevated
  • Total or free T3 — often elevated

The above tests may also be ordered periodically to monitor thyroid function and hormone production.

Laboratory tests used to help diagnose Graves’ disease and distinguish it from other autoimmune conditions may include one or more tests used to detect the presence of thyroid antibodies:1

  • Thyroid stimulating immunoglobulin (TSI) — the presence of this antibody is diagnostic for Graves’ disease.
  • Thyroid stimulating hormone receptor antibody (TRAb) — less specific than TSI
  • Anti-thyroid peroxidase antibody (anti-TPO) — this autoantibody is found in most people with Graves’ disease, as well as in Hashimoto thyroiditis.
     

If you are interested in adding TSI testing to your IMMULITE 2000 or 2000 XPi system menu, please contact the Inside Sales Department at (800) 242-3233, option 3.


Share this page:

1http://labtestsonline.org/understanding/conditions/graves/

2http://www.endocrine.niddk.nih.gov/pubs/graves/

The products/features (mentioned herein) are not commercially available in all countries. Due to regulatory reasons their future availability cannot be guaranteed. Please contact your local Siemens representative for additional information.