Fellowships and Preceptorships

For more information or assistance with registration, please call 1-888-221-8010, option 1, or email educationccainnovation.team@siemens-healthineers.com

Description: This three (3) day MR cardiovascular imaging program incorporates didactic instruction with practical, hands-on scanning and postprocessing sessions. Cardiovascular imaging basics will be presented, including CMR imaging physics and protocols. Clinical application will be emphasized through lectures ranging from normal anatomy to various states of cardiovascular pathology. Participants will spend time at the imaging console with volunteers at a 1.5T cardiovascular magnet. In addition, participants will study structural and functional cardiac MR evaluations utilizing current MR case specific applications, exploring cardiac morphology and function.

Key Topics

  • Indications, contraindications, and potential side effects of CMR
  • Practical knowledge in technical aspects of the CMR examination
  • Basic principles of MR Angiography and their applications
  • Recognize and minimize important image artifacts
  • Image post-processing techniques in clinical practice
  • Correlate CMR with other imaging modalities (echocardiography, nuclear cardiology, CCT, and interventional angiography), and with medical history, physical examination, laboratory, and hemodynamic data.
  • Recognize cardiac and vascular pathology (ischemia, infarction, value disease, congenital anomalies) on MRI examinations.

Description: The five (5) day Duke Cardiovascular MR Practicum provides the participant with an understanding of the principles of magnetic resonance imaging, safety issues in performing cardiac MR, and imaging protocols currently available for the evaluation of the structure and function of the cardiovascular system. Case presentations, one-on-one discussion, and observation of actual patient imaging will be emphasized. This course fulfills the SCMR requirements for Level 1 (Track B) and Level 2 certification and is aligned with the content for future CMR Board Exams.  

Key Topics

  • Cardiac Imaging
  • MRI Safety
  • MRI Physics – Pulse sequences and image reconstruction
  • Cardiac Imaging Sequences
  • Assessment of Ventricular Function
  • Assessment of myocardial viability
  • MR Perfusion Stress testing
  • Artifacts
  • Assessment of Pulmonary Veins
  • Parametric Mapping
  • Incidental Non-cardiac Findings
  • Role of CMR in Heart Failure and Cardiomyopathies
  • CMR Evaluation of ARVC/D
  • CMR Imaging of Patients with Implanted Cardiac Devices
  • CMR Image Analysis Tools
  • Congenital Cardiac Disorders
  • Assessment of the Peripheral Vascular Systems
  • Evaluation of the pericardium
  • Evaluation of Cardiovascular Hemodynamics
  • Case Studies


Location
Duke University
Durham, NC

Description

Tuition for (1) Physician to attend a (1) week-long rotation of the Cardiovascular MR Training Level 1 Program developed by the Duke Cardiovascular Magnetic Resonance Center (DCMRC). This course is designed to provide basic knowledge about the methods and applications of CMR in clinical cardiology. The participant will receive lecture materials on the underlying principles of MR physics which includes 13 hours of prerecorded lectures, the manifestations of specific cardiovascular abnormalities that are seen on CMR imaging and the imaging techniques used to differentiate the etiology of various abnormalities. Interesting case files as well as more than 10,000 clinical cardiovascular scans previously performed are available for review. Also included are observation of clinical cases and one-to-one discussion with faculty and staff on handling image acquisition and the interpretation of CMR scans. Physicians may participate in Level 1 training for 1-4 weeks.

Key Topics

  • Cardiac Imaging Techniques
    • CMR Methods and Applications
    • MR Physics
    • Cases Studies
    • Observation of clinical cases, handling image acquisition and interpretation of CMR Scans

Target Audience
This training is designed for the MR Physician seeking to advance their knowledge of MR cardiac imaging.

Location
Duke University
Durham, NC

Description

Tuition for (1) Physician to attend a (1) week-long rotation of the Cardiovascular MR Training Level 2 Program developed by the Duke Cardiovascular Magnetic Resonance Center (DCMRC). This course is designed to provide a comprehensive exposure to CMR imaging techniques focusing on the cardiac and vascular systems. It includes exposure to performance of CMR imaging, basic knowledge and understanding of CMR techniques, knowledge of MRI safety and patient screening, and advanced experience with interpretation of CMR scans. Physicians may participate in Level 2 training for 1-12 weeks.

Key Topics

  • Cardiac Imaging Techniques
    • Cardiac
    • Vascular
    • MRI Safety
    • Patient screening
    • Advanced experience and interpretation of CMR


Target Audience
This training is designed for the MR Physician seeking to advance their knowledge of MR cardiac imaging.

Location
Virtual Offering

Description

The two (2) Hour Virtual training consisting of any combination of interactions with an MRI technologist and/or physician for the purpose of providing information about the clinical application of a CMR procedure. The MRI technologist will review functionality, protocols and workflow and the physician will discuss issues related to interpretation of CMR scans and documentation of the findings. Training will be provided by a Duke technologist and a PhD or attending physician. The training is not meant to replace classroom instructions and, therefore, there is an expectation that the technologist and physician have at least a basic knowledge of CMR. Duke protocols covered during the training will be made available upon request at no extra charge.

Key Topics

  • Clinical application of CMR procedure
  • Cardiac functionality and workflow
  • Cardiac Protocols
  • Discuss issues related to interpretation of CMR scans and documentation of findings
  • Duke protocols available upon request

Target Audience
This virtual course is designed for MR Physicians, Technologists who are seeking to advance their knowledge of MR cardiac imaging.


Description: This three and one-half (3.5) day workshop hosted by Northwest Imaging Forums is for attendees interested in becoming an MR Medical Director/Physician (MRMD) or MR Safety Officer (MRSO) at their imaging facility. The workshop covers the basic principles underlying the potential areas of safety concern involved in the MR imaging process and magnetic resonance environment. In addition, defining the thought process algorithms for assessing whether a patient/device/implant/foreign object can safely undergo MR imaging, and familiarizing the attendee with medico-legal considerations associated with MR safety.

Key Topics

  • Static Magnetic Fields
  • RF Magnetic Fields
  • Gradient Magnetic Fields
  • Safety of Gadolinium-Based Contrast Agents (GBCA)
  • Cryogen Safety Considerations
  • Implant Safety: Clinical Application and Decision Making
  • Implant Safety: Kanal’s MR Safety Implant Risk Assessment App: Decision Tree Diagram and Utilization
  • Legal considerations

Contrast Disclaimer – A licensed physician may choose to use FDA-approved contrast agents in conjunction with an MRI exam, based on his/her medical opinion and discretion and in accordance with the instructions for use and indications for use supplied by the pharmaceutical manufacturer for the contrast agents.

Metal Disclaimer - The MRI restrictions (if any) of the metal implant must be considered prior to patient undergoing MRI exam. MR imaging of patients with metallic implants brings specific risks. However, certain implants are approved by the governing regulatory bodies to be MR conditionally safe. For such implants, the previously mentioned warning may not be applicable. Please contact the implant manufacturer for the specific conditional information. The conditions for MR safety are the responsibility of the implant manufacturer, not of Siemens.

Description: The two (2) day MR Safety Officer comprehensive course is designed to provide MR personnel with the knowledge to function in the role of an MR Safety Officer and to increase their knowledge regarding MR safety related issues. The course is based on the current ACR Manual on MR Safety, ACR Contrast Media Manual, FDA guidelines, IEC Standards, and the Examination Content Syllabus of the American Board of Magnetic Resonance Safety (ABMRS) credentialing exam. MR Safety, MR Zones, patient screening, proper patient attire, ferromagnetic detection, MR Magnets, and their components will also be discussed.

Key Topics

  • Static Field (B0)
  • Time-Varying Magnetic Field Gradients
  • Radio Frequency Field (B1)
  • Implants and Devices
  • MRI Environment, ACR, Quench
  • Screening and Patient Preparation
  • Ferromagnetic Detection
  • Contrast Media Safety
  • Patient Monitoring and Emergency Response

Contrast Disclaimer – A licensed physician may choose to use FDA-approved contrast agents in conjunction with an MRI exam, based on his/her medical opinion and discretion and in accordance with the instructions for use and indications for use supplied by the pharmaceutical manufacturer for the contrast agents.

Metal Disclaimer - The MRI restrictions (if any) of the metal implant must be considered prior to patient undergoing MRI exam. MR imaging of patients with metallic implants brings specific risks. However, certain implants are approved by the governing regulatory bodies to be MR conditionally safe. For such implants, the previously mentioned warning may not be applicable. Please contact the implant manufacturer for the specific conditional information. The conditions for MR safety are the responsibility of the implant manufacturer, not of Siemens.

For more information or assistance with registration, please call 1-888-221-8010, option 1, or email educationccainnovation.team@siemens-healthineers.com

Subscription Button Icon
Be the first to know about our events, training, and news