What Is Kidney Disease?Learn more about the types, symptoms, and risk factors

Kidney disease refers to any disease, disorder, or condition that affects the kidneys. While requirements and guidelines vary, imaging, laboratory diagnostics, and point‐of‐care testing are integral in screening, diagnosing, and/or monitoring most kidney conditions.

Siemens Healthineers offers solutions for healthcare providers, from primary‐care physicians and internists to nephrologists, oncologists, and radiologists, to improve the patient experience over a lifetime of the kidney healthcare continuum.

Chronic Kidney Disease

Chronic kidney disease (CKD) includes any condition that causes reduced kidney function for more than 3 months.3, 4

CKD is present when a patient’s glomerular filtration rate (GFR) remains below 60 milliliters per minute for more than 3 months or when a patient’s urine albumin‐to‐creatinine ratio is over 30 milligrams (mg) of albumin for each gram (g) of creatinine (30 mg/g).1


With early chronic kidney disease (CKD), people tend not to feel ill or notice any symptoms as kidney function deteriorates slowly over time. For this reason it has been referred to as the “silent killer.” Specific blood and urine tests are the only way to determine CKD.5

If kidney failure does occur, typical symptoms are weight loss and poor appetite, peripheral edema (swollen ankles, feet, or hands due to water retention), shortness of breath, blood or protein in urine, high blood pressure (hypertension), nausea, erectile dysfunction in men,6 vomiting, bone pain, headache, insomnia, itching, dry skin, malaise, fatigue with light activity, muscle cramps, high urine output or no urine output, recurrent urinary tract infections, urinary incontinence, pale skin, bad breath, hearing deficit, detectable abdominal mass, tissue swelling, irritability, poor muscle tone, change in mental alertness, and a metallic taste in the mouth.


Causes and Risk Factors

The two main causes of chronic kidney disease are diabetes mellitus and high blood pressure, which are responsible for up to two‐thirds of the cases. Diabetes happens when your blood sugar is too high, causing damage to many organs in your body, including the kidneys and heart, as well as blood vessels, nerves and eyes. When the pressure of your blood against the walls of your blood vessels is too high, it results in high blood pressure, or hypertension. If uncontrolled, or poorly controlled, high blood pressure can be a leading cause of CKD, heart attacks, and strokes. Also, CKD can cause high blood pressure.13

Other conditions that may lead to chronic kidney disease include3:

  • Diabetic nephropathy (diabetes can cause permanent changes, leading to kidney damage)
  • Systemic lupus erythematosus (SLE), a chronic inflammatory/autoimmune disease that can injure the skin, joints, kidneys, and nervous system
  • Prolonged urinary tract obstruction or blockage
  • Alport syndrome (an inherited disorder that causes deafness, progressive kidney damage, and eye defects)
  • Nephrotic syndrome (a condition that has several different causes, characterized by protein in the urine, low protein in the blood, high cholesterol levels, and tissue swelling)
  • Polycystic kidney disease (a genetic disorder characterized by the growth of numerous cysts filled with fluid in the kidneys)
  • Cystinosis (an inherited disorder in which the amino acid cysteine accumulates within specific cellular bodies of the kidney, known as lysosomes)
  • Interstitial nephritis or pyelonephritis (an inflammation to the small internal structures in the kidney)
  • Renal artery stenosis
  • Ascending (chronic) infections of the lower urinary tract

Other risk factors3:

  • Heart problems or stroke
  • Obesity
  • Family history
  • Tobacco use
  • 60+ years old

State

Qualitative Description

Renal Function (GFR)
mL/min/1.73 m2

1

Kidney damage – normal GFR

≥90

2

Kidney damage – mild ↓ GFR

60–89

3

Moderate ↓ GFR

30–59

4

Severe ↓ GFR

12–29

5

End‐stage renal disease

<15 (or dialysis)


Your doctor will want to pinpoint your diagnosis and check your kidney function to help plan your treatment. The doctor may do the following:

  • Calculate your Glomerular Filtration Rate (GFR). It is the best test to measure your level of kidney function and determine your stage of kidney disease. Your doctor can calculate it from the results of your blood creatinine test, your age, race, gender and other factors.
  • Perform an ultrasound or CT scan to get a picture of your kidneys and urinary tract. This tells your doctor whether your kidneys are too large or too small, whether you have a problem like a kidney stone or tumor, and whether there are any problems in the structure of your kidneys and urinary tract.
  • Perform a kidney biopsy under image guidance, typically ultrasound. This is done in some cases to check for a specific type of kidney disease, see how much kidney damage has occurred, and help plan treatment. To do a biopsy, the doctor takes a sample from the region of interest. The pathologist than performs the histological analysis.

In complex cases, your doctor may also ask you to see a kidney specialist who will consult on your case and help manage your care.

Acute Kidney Injury

Acute kidney injury (AKI) is a sudden, temporary, and sometimes irreversible loss of kidney function.1

In recent years, AKI has gained increasing recognition as a major risk factor for the development of chronic kidney disease (CKD). The clearest example of this relationship comes in cases of severe dialysis requiring AKI where patients fail to recover renal function. Indeed, acute tubular necrosis without recovery is the primary diagnosis for 2 to 3 percent of incident end‐stage renal disease (ESRD) cases annually. Yet this represents a small fraction of the renal disease burden resulting from AKI, as studies have demonstrated significantly increased long‐term risk of CKD and ESRD following AKI, even after initial recovery of renal function. Furthermore, this relationship is bidirectional and CKD patients are at substantially greater risk of suffering an episode of AKI. As a result, AKI is frequently superimposed on CKD and therefore plays a key role in CKD progression.2


There are a variety of symptoms that may include urinary hemorrhage, fever, weakness, fatigue, rash, diarrhea or bloody diarrhea, poor appetite, severe vomiting, abdominal pain, back pain, muscle cramps, no urine output or high urine output, pale skin, nosebleeds, swelling of the tissues, inflammation of the eye, and detectable abdominal mass.3 The symptom onset can sometimes be correlated to events like contrast application.


Causes and Risk Factors

Conditions that may lead to acute kidney failure3:

  • Myocardial infarction
  • Rhabdomyolysis (muscle breakdown)
  • Severe dehydration
  • Infection
  • Iodinated contrast agent
  • Administration or ingestion of certain medications that may cause toxicity to the kidneys
  • Renal artery stenosis
  • Conditions that may impair the flow of oxygen and blood to the kidneys, such as cardiac arrest

Diabetes mellitus and pre‐existing CKD are recognized as two major risk factors for AKI.2

Other Types

Other than chronic kidney disease or acute kidney injury, kidney disease may be characterized as end-stage renal disease or certain hereditary conditions.

There are many different types of hereditary kidney diseases, including congenital kidney and urinary tract malformations, congenital glomerulopathies, and tubular diseases.14

The three hereditary diseases with the highest incidence include:

  • Autosomal dominant polycystic kidney disease (ADPKD)
  • Congenital nephrotic syndrome of the Finnish yype (CNF)
  • Alport syndrome

End‐stage kidney or renal disease (ESRD) is the final stage of chronic kidney disease in which the kidneys no longer function well enough to meet the needs of daily life. People with diabetes or hypertension have the highest risk of developing ESRD.

It is important to note that one kidney can fail without any impact on overall renal function. MROI or nuclear medicine studies help to analyze renal function of left and right kidney separately. If kidney function is below 10% of normal and the damage is irreversible, the condition is called end‐stage renal disease or kidney failure. When the kidneys fail, the body retains fluid and harmful waste builds up. Two treatments are available for patients with ESRD: dialysis or transplantation.3


ADPKD is the most common hereditary kidney disease, with an incidence rate of about 1 in 1000. It is caused by mutations in the genes PKD1 and PKD2. A manifestation usually appears at the age of 30 to 50, and the clinical symptoms are hypertension, nephrolithiasis, and a progressive increase in the volume of both kidneys with appropriate accompaniments (e.g., impairment) due to massive cyst formation. Histologically, ADPKD is characterized by cysts in all areas in the nephron, which can vary in size and morphology. The most common extrarenal manifestations of the disease are cysts in the liver and pancreas.

The treatment of ADPKD is only symptomatic. Diseases that may negatively impair kidney function, like urinary tract infections, diabetes or arterial hypertension are usually treated or managed effectively. The larger the kidney volume, the worse the prognosis for renal function. In advanced stages, dialysis is indicated. A complete cure can be achieved only through kidney transplantation.8


CNF is an autosomal recessive disease, genetically caused by mutation of the nephrin gene NPHS1. The highest incidence is in Finland (1:10,000). The disease is characterized prenatally with an increase in the amniotic fluid alpha‐fetoprotein; at birth by massive proteinuria; and by increasing renal insufficiency after 6 months.

Symptoms include general persistent edema, ascites, and infections, and nutritional disorders are common because of the enormous loss of protein.

CNF is difficult and proceeds until the onset of ESRD. Corticosteroids and immune‐suppressants are ineffective for treatment. Dialysis and transplantation are therapeutic options.


Alport syndrome is an inherited disease resulting in a progressive deterioration of renal function and can affect the inner ear and eye, leading to hearing and vision loss.

Its incidence is 1 in 10,000, and it is caused by mutations in the genes COL4A3, COL4A4, and COL4A5, which encode protein chains of collagen type IV. This leads to a  dysfunction of basal membranes, which is especially critical in the glomerulus, the inner ear, and the eyes.

The disease can be autosomal dominant (5%), autosomal recessive (15%), and is X‐linked in 80% of cases. Boys and men are more affected.

After birth, the urinalysis is abnormal because of proteinuria and hematuria. This is an expression of an incipient chronic glomerulonephritis. Treatment options are ACE inhibitors or AT1 receptor antagonists. This therapy delays the manifestation of terminal kidney failure, but it cannot be stopped. The progressive renal failure may require hemodialysis or transplantation.

1
2
3
4
5
6
7
8
9
10
11
12
13
14
Subscription Button Icon
Be the first to know about our events, training, and news