Cardiac Troponin

Myocardial Muscle Tissue
Myocardial Muscle Tissue

Videos: High-Sensitivity TnI & Point-of-Care hsTnI

 

Troponin, a complex of three contractile regulatory proteins, troponin C, T and I, controls the calcium-mediated interactions between actin and myosin in cardiac and skeletal muscles. Troponin-I and T are specific to cardiac muscles, unlike troponin-C which is associated with both cardiac and skeletal muscles. Hence, troponin-C is not used in the diagnosis of myocardial damage.1
 

Cardiac troponins are released into circulation in response to myocardial necrosis. As such, cardiac troponins are the preferred biomarkers for the detection of cardiac injury1, and have long assisted physicians in improving diagnostic strategies for the effective management of patients with chest pain.

  

Background

  • Relatively non-specific markers of myocardial damage, such as creatine kinase (CK), creatine kinase-MB (CK-MB), and myoglobin (MYO), were used in diagnostic laboratories prior to the commercial release of the troponin assays.
  • Numerous clinical studies on troponin have indicated its superior cardiac specificity in comparison to CK, CK-MB, or MYO.
  • Troponin levels remain elevated in the blood longer than CK-MB or MYO, providing an extended diagnostic window for MI.

Cardiac Markers: Approximate Levels vs. Time of Onset Post MI

Troponin Graph

Troponin testing and the definition of Myocardial Infarction has rapidly evolved ever since the release of the first commercially available troponin assay in 1997.

Learn more.

 

Clinical Applications

The clinical utility of troponin-I has expanded over the years due to better understanding of the significance of cTn-I in myocardial damage.


Cardiac Troponin-I (cTn-I) in Acute Coronary Syndrome (ACS)

 

Cardiac troponin has advanced from its initial application in the diagnosis of acute myocardial infarction (AMI) to include risk stratification of patients with ACS, with respect to the relative risk of mortality and therapy orientation.

  • It estimates the probability of a patient having an adverse cardiac event in the next 30-60 days.
  • It is applicable to patients diagnosed with unstable angina (UA), non-ST segment elevation MI (NSTEMI), and chest pain.
     
Troponin

Cardiac Troponin-I (cTn-I) in Myocardial Infarction (MI)

 

Elevated levels of cardiac troponin are used to diagnose MI in the presence of myocardial ischemia

 

The 2000, 2007, 2012 joint European Society of Cardiology (ESC), American College of Cardiology Foundation (ACC), American Heart Association (AHA), and World Heart Federation (WHF) expert consensus document for the universal definition of myocardial infarction defines an elevated troponin level as:

  • A measurement exceeding the 99th percentile of a reference control group of normal, non-diseased individuals in the presence of ischemia.2 
Protonin

The consensus document also recommends for the universal definition of myocardial infarction that:

  • The imprecision of troponin assays used in diagnosing MI be ≤10% coefficient of variation (CV) at this 99th percentile.2

 

The National Academy of Clinical Biochemistry (NACB) and International Federation of Clinical Chemistry (IFCC) committee supports the joint recommendations of the ESC/ACC/AHA, with the recognition of one additional point.

  • Imprecision of <25% at the 99th percentile does not lead to significant patient misclassification if a series of timed (serial) troponin orders are used.3

 

Troponin

Non-MI Causes of Elevated Cardiac Troponin-I Levels

 

cTn-I levels are also elevated in conditions representing ongoing myocardial damage due to non-ischemic etiologies. Examples include:

  • Myocarditis
  • Pulmonary embolism (PE)
  • Stroke


The elevated levels of cTn-I in all the above conditions possess a high prognostic value in relation to morbidity and mortality, irrespective of the cause.4

Interpretation of Cardiac Troponin-I Levels2,5

Graph

Impact on Management

Cardiac troponin-I assays have made a tremendous impact on the management of ACS as they facilitate risk stratification and early diagnosis of ACS, thereby improving patient care and outcome. The key benefits of the troponin-I assays include:

  • Identifying patients at high risk, either at short- or long-term follow-up
  • Justifying the need for more aggressive treatment
  • Identifying patients who would benefit from aggressive thrombolytic treatment since elevated troponins are associated with an active thrombotic process.6

 

Reliable Answers to Critical Cardiac Questions

Siemens Healthcare Diagnostics is the only company offering multiple solutions for high-sensitivity troponin I* testing that meets the current guidelines for MI diagnosis.

Learn more

 

 

 

*Defined by the ESC/ACC committee as an imprecision level of ≤10% at the 99th percentile of normal.

 

 

References:
1. Babuin L, et al. CMAJ. 2005;173:1191-202
    http://www.pubmedcentral.nih.gov/articlerender.fcgi?tool=
    pubmed&pubmedid=16275971
2. Thygesen K, et al. J Am Coll Cardiol. 2007;50:2173-95.
    http://content.onlinejacc.org/cgi/content/short/50/22/2173
3. Apple FS, et al. Clin Chem. 2007;53:547-51.
    http://www.ncbi.nlm.nih.gov/pubmed/17384000?ordinalpos=2&
    itool=EntrezSystem2.PEntrez.Pubmed.Pubmed_ResultsPanel.
    Pubmed_Default ReportPanel.Pubmed_RVDocSum
4. Wu AHB, et al. Clin Chem. 2007;53:2086-96.
    http://www.clinchem.org/cgi/content/abstract/53/12/2086
5. Bassand JP, et al. Eur Heart J. 2007;88:1598-660.
    http://eurheartj.oxfordjournals.org/cgi/content/full/28/13/1598
6. Morrow DA, et al. Clin Chem. 2007;53:552-74. (CVD brochure)
    http://www.clinchem.org/cgi/content/full/53/4/552
 

Did this information help you?
Thank you for your response
We detected numbers and/or an '@' symbol in your comment. Are you trying to enter a phone number or email address so that we may contact you, please contact us via our email form instead.

Note: to get a direct personal response, please contact us via our email form.

Thank you

Close share layer

Share this page